AI on the Edge with STM32
By Michael Parks, PE, for Mouser Electronics
Published November 14, 2022
For decades, engineers and technicians have relied on “best guess” models built on stress testing
components to plan and schedule preventative maintenance for complex systems. While nothing inherently wrong
with this concept, it was still possible for premature breakdowns to occur (hardware failures often follow a
so-called bathtub curve of failure likelihood over time). Conversely, it can be a waste of resources (financial,
manpower, materials) to perform maintenance on systems that do not require any maintenance. Predictive
maintenance (PdM) is changing that by making maintenance decision-making a data-driven process. Key to that are
embedded devices driven by Machine Learning (ML) algorithms that can sense, process and communicate the
indicators of health for any given system of interest. Though historically developing ML-based solutions have
been a cumbersome process at best. STMicroelectronics (ST) is tackling that challenges that systems engineers
face when developing predictive maintenance capabilities through unique hardware and software solutions.
First, their B-U585I-IOT02A Discovery Kit is a powerful development platform right out of the box. It features
the STM32U585AI microcontroller, built around an ARM Cortex-M33 core, 2 Mbytes of Flash memory, and 786 Kbytes
of SRAM. In addition, because this board is geared toward developers building Internet of Things (IoT) products,
it hosts a bevy of sensors that can be easily accessed, including microphones, temperature and humidity,
magnetometer, accelerometer, gyroscope, pressure, time-of-flight, and gesture-detection sensors. If you have
custom hardware you wish to test and integrate; the dev board also features standard hardware interfaces such as
the Arduino Uno V3 shields, STMod+, and Pmod. Finally, it wouldn’t be an IoT dev kit without the onboard
Wi-Fi and Bluetooth modules.
Of course, hardware without software is like a vehicle without fuel. Developing ML software tailored to your
STM32 hardware is straightforward thanks to the NanoEdge AI Studio platform, available for both Windows and
Ubuntu Linux. Studio features a wizard-like interface that walks you through five steps needed to target the ML
algorithms to the target STM32-based development kit. Data to train the model can be uploaded from a file or
real-time from the target development board. It’s a flexible and straightforward way to train, build, and
test anomaly detection or classification ML algorithms.
Project Materials and Resources
The project is centered around the STM B-U585I-IOT02A Discovery development kit. It has been designed
specifically for industrial applications that need to leverage ML technology featuring numerous onboard sensors
for convenient training of ML algorithms and running inferencing engine during deployment. We will leverage the
onboard ISM330DHCX, an industrial-focused system-in-package 3D accelerometer and gyroscope that offers
convenient digital output over a wide range of acceleration and angular acceleration values, very useful for the
project that will be detailed in this article
Bill of Material (BOM)
You can click this Mouser
project share link to access the BOM and the current pricing. As of the date this article was initially
written, the BOM cost is about $65 (USD) before applicable taxes and shipping costs. Table 1
lists the items in the BOM.
Table 1: IOT2A NanoEdge AI Studio BOM
Quantity
|
Mouser P/N
|
Description
|
|
1
|
511-B-U585I-IOT02A
|
Development Boards & Kits - ARM Discovery kit for IoT node with STM32U5 series
|
Project Resources
All source files for this project are located in this GitHub repository. The repository is divided
into two main folders:
Documentation
The documentation folder contains graphic files of schematics and other necessary reference materials.
Software
The Software folder contains the source code. More details about these files can be found in the
Software section
below. The two main directories are as follows:
iot2a_neai_training_application: Contains the codebase for an application that reads the
accelerometer data
and formats it in a manner that is ready for consumption by the ML training module (aka Signals) inside the
NanoEdge AI Studio application.
iot2a_inferencing_application: This contains the inferencing engine code generated by the
trained ML model.
It can be used for a project that responds to the three-axis accelerometer data onboard the B-U585I-IOT02A
Discovery development kit.
Tools
This project assumes that you have access to the following tools:
- Computer with a high-speed Internet connection, running Windows 10, Windows 11, or Ubuntu Linux.
Building the Project
Industrial facilities rely heavily on fans for a variety of purposes. Keeping air moving is critical to maintain
temperature, remove particulate matter from the air, remove odors, and to remove moisture to name a few. Failure
of the motor or a fan blade can have severe consequences for industrial operations. This project will
demonstrate how ML can be used to determine the operating status of a fan by detecting changes in the housing
vibrations of the fan from a controlled baseline. The following section will examine the necessary steps to get
your project up and running. This section is broken down into the following subsections:
- Connecting the Development Kit to Development Computer
- Setting up the Software Development Toolchain
- Software Development: Training Application
- Software Development: Inferencing Application
- Project In Action
From a product engineer's perspective, developing ML-powered devices can be broken into three major steps. First,
collecting training data and classifying it. Next, taking the training data and creating the neural network and
benchmarking its performance, tweaking as necessary. Lastly, deploying the code to endpoint devices and
inference, which is just a fancy way of saying using the ML model in the real world with live data not used for
training or testing/benchmarking.
Connecting the Development Kit to Development Computer
The B-U585I-IOT02A Discovery development kit (Figure 1) has three USB interfaces for different
purposes. First, a USB-C interface (CN1) for powering the board during normal operations. Second, a micro-USB
connector (CN12) to update the onboard Bluetooth module. Lastly, a second micro-USB port (CN8) that allows us to
program and debug the STM32U585AI microcontroller via the onboard STLINKV3E in-circuit programmer/debugger. No
external hardware is needed!
Figure 1: The B-U585I-IOT02A Discovery development board contains numerous
on-board sensors to develop ML applications. Programming and debugging are conducted over the USB port
located along the right side of the board. (Source: Green Shoe Garage)
IMPORTANT NOTE FOR WINDOWS USERS: Before connecting the B-U585I-IOT02A Discovery development
kit, it is necessary to download drivers from the ST website in order to interact via the STLINK-V3E. Failure to
do so might result in the development board not being properly enumerated in the virtual COM ports list.
Once the drivers have been installed, plug the USB cable into the computer and the development board. Next, a
micro-USB cable should be plugged into the micro-USB port along the right side of the development board
(connector CN8). Finally, the power indicator LED and UART communications LED should ignite, and if on a Windows
machine, a pop-up should announce the detection of the B-U585I-IOT02A Discovery development board attached to
the system.
Setting up the Software Development Toolchain
The project consists of two software applications. The first is a C++ application that will serve as a datalogger
to take the sensor data from the development board and send it to the training tools of the NanoEdge AI Studio.
This application will be written using the ARM Keil Studio Cloud integrated development environment (IDE). A
free account can be set up here. For this project, we first need to set
up a data logger that reads the three axes of the accelerometer. Then, we will collect three different datasets.
The first will show the fan in the off position. The second will show the fan in a failure mode induced by an
object obstructing blade rotation. The third and final dataset will show the fan under normal operating
conditions.
NanoEdge AI Studio is available for Windows 10 and 11 and Ubuntu Linux. As of the date this article was written,
the current version of Studi0 3.0 and a 90-day free trial version can be downloaded from here. But, again, download
the STLINK drivers first, as discussed in the previous section, "Connecting the Development Kit to Development
Computer."
ARM Keil Studio Cloud (Figure 2) is a web-based IDE and should work in any modern browser. We
used a Chromium-based browser with all the latest updates installed for this project.
Figure 2: The Keil Cloud IDE offers a convenient way to program your
development board from anywhere in the world via a Chromium-based browser. (Source: Green Shoe Garage)
Software Development: Training Application
The codebase for this project is written in C++. First, we must create a small datalogger application that will
send the accelerometer data from the development board to the NanoEdge AI Studio training software. For testing
purposes, we will produce the following datasets for training:
fan_off: This data set contains the accelerometers' values while the development board is
connected to the
fan and the fan is not running. The accelerometers will output X, Y, and Z acceleration readings at or near
0g.
fan_normal: This data set contains the accelerometers' values while the fan is operating in a
normal manner.
The X, Y, and Z acceleration readings will be fairly consistent, with a gradual ramp up and ramp down as the
fan turns on and turn off.
fan_failure: This data set contains the accelerometers' values that were recorded while
inducing a
mechanical failure caused by preventing the fan from rotating normally. The X, Y, and Z acceleration values
will change randomly and quickly.
Of course, if you wanted more nuanced outputs (a.k.a. signal classes), you could create additional training
datasets. However, for simplicity of explanation, we are keeping with these three states.
Before accessing the onboard ISM330DHCX accelerometer, we have to download the drivers from the ST GitHub
repository. Unfortunately, it is currently unavailable in the standard board support package (BSP) folder for
the B-U585I-IOT02A Discovery development board. To clone or download the ISM330DHCX library, click here.
AN IMPORTANT NOTE ON PREPARING SIGNAL FILES: Correctly capturing the signal generated by the
phenomenon of interest is crucial to training a reliable ML model. A signal file is made by discretely sampling
the continuous sensors signal over a short, finite span of time. Recall that the Nyquist criterion dictates that
a signal be sampled at twice the rate of the highest frequency component of the signal of interest. Failure to
do so could result in false positive or negatives due to the aliasing effect. For more information on
collecting training data and formatting the training and test data files, please visit AI:NanoEdge AI Studio
- stm32mcu
Key Files
The critical files for this project include:
main.cpp: Contains the code that generates the UI and contains the callback code that triggers
when an event
occurs (such as screen open, button pressed, etc.)
ism330dhcx.c/.h: These are the driver files for the onboard ISM330DHCX accelerometer. The
functions contained within
these files allow for the developer to manipulate accelerometer settings and to read the acceleration values
while the device is in operation.
Key Variables and Constants
You might want to be aware of a few variables and possibly tweak them depending on your particular design
choices. These variables can be found in the file titled main.cpp:
ISM330DHCX_Object_t ism330dhcx_object: An object that allows us to communicate with the onboard
accelerometer.
ISM330DHCX_AxesRaw_t acc_values: An enumerated data type that consists of three uint_16_t
values for the x,
y, and z axes.
float x, y, z: A place to store the accelerometer values locally within main.cpp.
static int32_t ISM330DHCX_Probe(void): Mechanism to get and set settings of the onboard
accelerometer.
Key Functions
The main.cpp file contains the initialization code, the main loop, and support functions for the
project. The
support functions include:
ISM330DHCX_ACC_Enable(&ism330dhcx_object): Turns the accelerometer hardware on. Failure to
do so will
result in garbage data. Must pass a pointer to the ism330dhcx object.
ISM330DHCX_ACC_GetAxesRaw(&ism330dhcx_object, &acc_values): Mechanism to request the
accelerometer
data. Must pass it a pointer to the ism330dhcx object and a point to the enum data structure to store the x,
y, and z axes data.
Software Development: Inferencing Application
Now that the data logger application is complete, it's time to develop the inferencing application that will
detect the real-time motion or no motion onboard the development board. The codebase for this part of the
project is also written in C++. This is where the NanoEdge AI Studio (Figure 4) shines. It
presents a straightforward, five-step process to build, test, and deploy a function inferencing engine for any
supported STM32 hardware platforms and sensors. A quick glance at the five steps are as follows:
- Project Settings: Declare which development board and sensors you intend to utilize.
- Signals: Collect model training data from a file or streamed via a serial connection
directly from the development board.
- Benchmark: Create the ML model and test its accuracy and memory footprint.
- Emulator: Test the model using independent test data.
- Deployment: Create the inferencing application that can run on your target device.
Figure 3: NanoEdge Studio AI isa powerful tool to train, test, and deploy ML
algorithms to embedded devices. (Source: ST)
To begin, let's launch the Studio application on our development machine. This will present us with four types of
ML algorithms we can build. They are:
- Anomaly Detection: Used for detecting anomalies in data using a dynamic model.
- 1-Class Classification: Used for detecting anomalies in data using a static model.
- N-Class Classification: Used for distinguishing among n different states using a static
model.
- Extrapolation: Used for estimating an unknown target value using other known parameters,
using a static model.
For this project, we will select the n-class classification model. Next, select Create New Project.
This will
begin the workflow, starting with the Project Settings step.
Figure 4: Training an ML model begins with selecting the target devices and
preferred sensors. (Source: ST)
Project Settings
The first step in the process is to select our target development board and from which onboard sensors we will
collect data (Figure 5). The following selections should be made:
- Name: Assign a title for this particular project.
- Target: The target development board, in this case, selects the Disco-B-U585I-IOT02A.
- Sensor Type: Select Accelerometer 3 axes.
Figure 5: NanoEdge AI Studio provides multiple ways to get training into the
ML model training engine. Here the data is being streamed real-time from the Discovery kit development board
via USB serial. (Source: Green Shoe Garage)
Signals
The second step in developing the ML model is to collect real-world training data from the chosen development
board (Figure 6). To do so, we will follow these steps:
- Click on
ADD SIGNAL.
- Select
FROM SERIAL (USB).
- Select the correct COM port and baud rate, in this case, 9600bps.
- Place a checkmark in the
Maximum number of lines checkbox and enter 100 lines.
- Click on the
START/STOP button. Wait for all 100 data points to be collected. You should see
the data coming in via
the Serial output text box and charted graphically.
- Click
CONTINUE to preview the data.
- Ensure the delimiter type is
space.
- Click on
IMPORT.
- Give the dataset a name in the
name text box (e.g., no_motion, at_rest, etc.)
- Click on
RUN OPTIONAL CHECKS to have Studio verify that there are no common errors in the
dataset.
Figure 6: : NanoEdge AI Studio provides a benchmarking tool to determine the
accuracy of the ML model as well as its memory footprint. (Source: Green Shoe Garage)
Benchmark
Next, Studio will generate a neural network model and then run a benchmark against the datasets to see how well
the model tracks against the training data (Figure 7). It will report an accuracy score, a
confidence score, and how much RAM and flash memory the model will consume on the target board. To run the
benchmark, do the following:
- Click RUN NEW BENCHMARK.
- Place a checkmark in each of the signal classes you want to benchmark.
- Use the slider to adjust the number of CPU cores you wish to dedicate to the benchmark. The more cores, the
faster the benchmarking, but it might make your machine sluggish, depending on the size of the dataset.
Figure 7:: To verify the performance of the ML model, Studio provides both a
browser-based emulator and an emulator that can be ran locally to verify performance against test data vice
the training data. (Source: Green Shoe Garage)
Emulator
Now that we have a working model, we can run an emulator to test that model against new testing data to see how
it performs against datasets not used for training (Figure 8). In short, we can see how well
the model works in the real (albeit emulated) world. Again, test data can be uploaded as a text file or streamed
in real-time from the target development board via USB. To emulate the ML model, follow these steps:
- Select the benchmark you wish to emulate.
- Click
INITIALIZE EMULATOR. Alternatively, you can run the emulator locally on either a Linux or
Windows
machine. Next, select the emulator appropriate for your computer's operating system.
- Select the correct COM port and baud rate (again, 9600bps for our code).
- Click the
START/STOP button.
Figure 8:: Once a developer is satisfied with the performance of the ML
inferencing engine, the model can be deployed to target hardware with just a few mouse clicks. (Source:
ST)
Deployment
The final step is to generate the firmware that can be run on the target board for inferencing on the actual
target hardware (Figure 9). Again, there are a few options (compilation flags) that can be
selected by placing a check in a checkbox. Those options are:
- Multi-library: Check the box if you want to integrate more than one
NanoEdge AI library in your program. Then, choose a suffix for each library.
- Float abi: Specifying soft causes GCC to generate output containing
library calls for floating-point operations. "hard" allows the generation of floating-point instructions and
uses FPU-specific calling conventions.
- fshort-wchar: The "
-fshort-wchar" option can improve memory usage, but might
reduce
performance because narrow memory accesses can be less efficient than full register-width accesses. The
default is "-fno-short-wchar." That has the default size of wchar_t at 4 bytes.
- fshort-enums: The "-fshort-enums" option can improve memory usage but might reduce
performance because narrow memory accesses can be less efficient than full register-width accesses. The
default is
-fno-short-enums. That is, the size of an enumeration type is at least 32 bits
regardless of the
size of the enumerator values.
We will leave the options alone for now. When ready to generate the inferencing engine code, follow these steps:
- Select which benchmark you wish to generate the code against, by selecting the appropriate benchmark from
the dropdown menu.
- Click
COMPILE LIBRARY to generate the code and download the .ZIP file containing the
inferencing code.
- Copy the "hello world" application generated and paste it into your main.cpp inferencing application file.
Project in Action
With the project assembled and firmware installed, it's time to verify the operation of the inferencing engine.
Plug the USB cable into the device as you did for programming and debugging earlier. Set the board on the lab
bench and fire up a serial terminal such as PuTTY. Ensure that the
development board is placed on the fan at the same location the datalogger was connected for collecting training
datasets. Failure to do so could result in false positives and negatives. As a general suggestion, placing the
accelerometer slightly off center axis of rotation seems to result in the best results.
Ensure that the correct COM port is chosen and set the baud rate to 9600 bps. Data from the inferencing engine
will begin to stream over the serial port within a few seconds. The critical values to look out for include:
- class_name: The name of the class (e.g.,
in_motion, at_rest) that
the inferencing engine
believes is currently happening.
- class_status: The numeric identifier of the class.
- class_probability: The probabilities of all enumerated classes. Use the class_status value
as the index into the list of possible probabilities to determine the probability of each class.
For this example, we allow the fan to operate normally, and the inferencing engine determines that the
accelerometer attached to the fan is detecting normal motion and gives us a probability of 99.97% chance that
the correct class has been selected (Figure 10). We have also chosen to light a user-definable
LED (attached to GPIO_Pin_7) when the most likely class (above 80% probability) is the
fan_normal class.
Figure 9:: The accelerometer inferencing engine in action. Streaming the
output of the inferencing engine via USB serial is a convenient way to verify performance and debug your
application. (Source: Green Shoe Garage)
Armed with these new insights into our fan’s health we can begin to establish proactive maintenance
procedures that are triggered when the system sends notifications that it is detecting aberrant behaviors. In
our example (Figure 11), that could be as simple as dispatch a technician if the fan is in the
fan_failure state for more than ten minutes.
Of course, there are numerous other use cases for such ML-enabled PdM. Consider the following examples:
- Measuring current through a breaker to analyze current draw as a part of machinery health analysis or an
energy management program.
- Sensing and analyzing fluid flow rates in a piping system to detect blockages that could lead to costly
environmental remediation if there were to be a spill.
- Detecting the anomalous temperature, humidity and vibrations within a refrigerator would be very useful to
predict imminent failure. This could help save significant money for restaurants by avoiding spoilages.
Figure 10:: Experiment with location of the accelerometer to optimize
results. (L) Placing dev board on top of fan motor housing. (R) Placing dev board on face fan cage. Placing
dev board on the motor housing seemed to work best. (Source: Green Shoe Garage)
Predictive maintenance, powered by smart technology solutions like STM's IoT02A Discovery Kit and their NanoEdge
AI Studio is changing how we plan, inspect, maintain, and repair industrial machinery. Reducing downtime while
also optimizing resource utilization (technician’s time, money, materials) means industrial operations can
“have their cake and eat it too”. Maintenance does not have to be reactive or based on statistical
models. Nor does maintenance need to be done “just to be safe.” Machine learning algorithms, when
couples with low-cost, yet powerful embedded systems can truly deliver us a world of smart, predictable
maintenance. And that world is here, today. For more information on STM’s IoT02A Discovery Kit and their
NanoEdge AI Studio, please visit here. B-U585I-IOT02A Discovery Kit -
STMicro | Mouser
Author Bio
Michael Parks, P.E.
is a contributing writer for Mouser Electronics and the owner of Green Shoe Garage, a custom electronics design
studio and technology consultancy located in Southern Maryland. He produces the S.T.E.A.M. Power Podcast to help
raise public awareness of technical and scientific matters. Michael is also a licensed Professional Engineer in
the state of Maryland and holds a Master's degree in systems engineering from Johns Hopkins University.