Advancing the Smart Factory Through Innovation
By Karl-Heinz Steinmetz, Texas Instruments
Advancements in intelligent electronic sensing, control and communication are enabling new levels of factory
automation for greater efficiency and lower operational costs — and ultimately delivering better products
to customers.
Today, in all regions of the developed world, manufacturing is changing rapidly. So rapidly, in fact, that some
say we are undergoing a fourth industrial revolution. While the introductions of steam power, the assembly line
and early automation drove the first three industrial revolutions, machine intelligence will fuel the fourth
one. Advances in electronic intelligence make it possible, to an extent undreamed of in the past, for equipment
to measure and modify processes, and for factories to communicate over a wide area. The transition promises a
number of benefits, including greater efficiency, flexibility, quality and safety, as well as improved
maintenance, energy savings and lower production costs.
The importance of the shift to a new manufacturing system, or the smart factory, cannot be overemphasized. In the
future, all forms of advanced industry will have to become more intelligent in order to compete effectively.
This intelligence comes from advanced integrated circuits (ICs) that provide sensing, measurement, control,
power management and communication, both wired and wireless.
Equipment manufacturers will introduce or add more of these sophisticated electronics in order to enhance
assembly, chemical processes and other stages of manufacturing. Sensors throughout the manufacturing area,
powered by harvested energy, will report on conditions continually through wireless communications via the
Internet "cloud." Programmable logic control (PLC) units and software will grow in importance, along
with complex systems that govern the entire factory floor and exchange information with operations elsewhere.
As an end-to-end supplier of advanced electronic solutions for industrial systems worldwide, Texas Instruments
(TI) plays an important role in providing differentiating ICs, software and support that will transform industry
in the years ahead.
Benefits of the smart factory
Traditionally, factory automation has been optimized to produce identical or nearly identical goods efficiently
and rapidly to achieve cost reductions from volume production. Product variation and design changes often
require some degree of flexibility be built into the process. This flexibility usually requires down time for
resetting equipment and retooling, which can diminish volumes and increase costs. To the extent necessary,
quality, reliability and safety are also built into the process, though these positive factors often represent
short-term costs, even if they provide long-term value.
Greater electronic intelligence can enhance the manufacturing process to provide flexibility while keeping costs
low and improving quality, reliability and safety. Product diversity is generally market-driven, and often the
more the product line can be varied, the more competitive it can be. When intelligent equipment in the factory
can handle product variations automatically, smaller production runs become possible without significantly
increasing production costs. In this way, smart factories allow greater product diversity and facilitate shorter
life cycles for products that have to change rapidly.
To achieve this level of flexibility, intelligence must be built into even the smallest steps of the process. In
car manufacturing, for instance, there may be more than two million individually orderable configurations of the
finished good, and countless changes in assembly may be needed to cope with all the variations. Even a seemingly
straightforward tool such as a screwdriver needs to automatically adapt its torque limitation to the part, which
may be steel, carbon or plastic in different configurations. In another example, the increasing use of 3D
printers carries flexibility to an extreme, since these can readily adapt to creating prototypes, a small run of
items, or even mass production with changes in materials.
Communications is an essential part of the picture, too. Intelligent processes can adapt to product needs based
on data entry in the business office, or even unit by unit according to sales orders, for immediate response to
customer demands. Moreover, when more significant process changes are necessary, they can often be made quickly
through programming, providing a fast, inexpensive way to improve quality or incorporate the results of field
reliability studies without the need for expensive retooling.
Intelligent monitoring also enables better predictive maintenance, enhancing the stability and safety of the
production process. Vibration sensing, for example, can give an early warning when motors, bearings or other
equipments are in need of maintenance. Maintenance also can be scheduled more efficiently through automatic
monitoring and reporting, keeping assembly lines in operation. Well-maintained machines are also safer for
workers, and there are other safety benefits that can result from more intelligent equipments as well. For
instance, today a robot arm must be in an enclosed area in order to avoid striking human workers. In the future,
sensors and control intelligence will direct a robot to stop or do an alternative task if a human is within
reach. Safer robots will also find new uses, such as teaming with human workers to move and place heavy items.
The above factors can increase product value, decrease production costs, or both. More flexible processes enable
low-volume, even one-of-a-kind production runs that are cost-effective and permit manufacturing of diverse
products that more people want and will pay more to have. Direct production line communications with business
operations enhances just-in-time supply maintenance, which along with well-maintained equipment, keeps lines
running more smoothly and reduces costs. A safer environment also benefits labor and can minimize damage claims
against management.
The smart factory represents a fundamental change in how production processes are set up and organized. The smart
factory also serves to decentralize manufacturing, provide greater intelligence where production activities take
place, and create an overall system that is cognitive and self-healing. In addition, the changes coming with the
next industrial revolution are not strictly limited to what is traditionally considered manufacturing. Rather,
what is envisioned is a system of learning and adaptation that can cover the whole product life cycle, from
engineering and production, to maintenance and upgrading, to disassembly and recycling. Electronic intelligence
at every stage of this chain can add value to the product, improve customer satisfaction, and achieve broader
goals such as saving energy and reducing material waste.
Technology requirements for the smart factory
For manufacturing equipment makers and system integrators, the smart factory represents a golden opportunity.
Virtually every stage of an advanced manufacturing process can benefit from the addition of automated sensing,
control intelligence and communications. (Figure 1.)
Figure 2: Sensor, control, interface and communication
technologies based on analog and embedded processing, will work together to advance the smart factory of the
future.
From an IC perspective, the base technology already exists, and much of it is already in use and factory-tested.
What is needed to implement the smart factory are standards, optimized production equipments, and system
integration at the factory level and beyond. As these are developed, and as more systems are deployed, dedicated
silicon will increasingly be developed to support these applications and fuel growth.
The intelligence requirements for intelligence in automated manufacturing vary, depending on the specific
application. Programmable logic control (PLC) in a robot, or for a series of motors operating an assembly belt,
usually requires a high level of processing, together with high-bandwidth wired communications. These
requirements increase for the nodes that govern an entire assembly line or factory floor, where the
computational and communications performance required may equal or surpass that of computer nodes in
conventional local-area networks.
On the other hand, one of the marked differences of the new automation is that smart factories will employ
numerous sensors in areas where it is expensive or even dangerous to run wiring. These sensors will have to
communicate wirelessly to base stations or through the Internet cloud, in a way similar to what is available in
the consumer world through the Internet of Things, but with additional requirements to withstand industrial
stresses and ensure robust communications. The sensor units will either have to operate for years on a battery,
or will have to harvest small amounts of energy from vibrations, light, heat differentials or ambient radio
waves. These sensor ICs will need to be designed to minimize power consumption, and specialized components for
power management must also be designed to work with each system effectively.
Trends at the heart of automation
Sensors are the eyes and ears of the smart factory, and as such they will be everywhere. Besides conserving
power, embedded sensing systems must be small, inexpensive and rugged, with industrial qualification for
vibration and temperatures up to 125ÂșC. The analog front end (AFE), requiring integrated fault detection,
consists of a sensor-transducer for temperature, pressure, humidity, position, motion, power, gas/chemical or
something else, plus signal conditioning and analog-to-digital (A/D) signal conversion. Microcontrollers (MCU)
are needed to perform analytics and control, possibly relying on ferroelectric memory (FRAM) for non-volatile
storage that can be written to quickly and far more often than flash memories. Today there is a trend toward
developing the lowest-power single-chip sensor node, which will integrate all of these functions.
Another trend is to create sensors capable of performing additional functions, changing them from dedicated
devices that transmit only one kind of information into fully configurable monitors with hot plug replacement
capability. To adapt to this greater functionality, sensor manufacturers may need to acquire new intellectual
property. At a minimum they need to develop and offer higher complexity products, including necessary services
like tools and cloud services.
Communications, both wired and wireless, is frequently the gating factor in systems for automated manufacturing,
since it determines the amount of computation that can be employed
and often defines power requirements. Future communications modules will have to operate on less power, be more
highly integrated and offer greater flexibility in terms of protocol support, power schemes and peripherals.
Increased bandwidth will also be important, especially for wired communications, pointing to greater use of
Gigabit Industrial Ethernet, along with integrated protection schemes to comply with industrial standards.
In sum, the challenges facing those who create factory equipment and integrate smart factory systems include the
very limited power budgets involved, the need for reliability and stability of the wireless links within factory
automation and process control environments, the higher level of complexity of both hardware and software, and
the need to maintain secure systems for protection of the overall system from outside interference.
TI technology and solutions for smart factories
Industrial customers require a secure supply chain with assurance of long-term deliveries, high quality standards
and reasonable pricing. In addition, industrial applications have special technical requirements that demand a
long-term strategy with support for standards, silicon qualifications and software. TI has become one of the
world's leading industrial IC suppliers by recognizing the market needs and responding through products, support
and manufacturing, as well as by building special team relationships with its major customers.
TI is the only semiconductor supplier to offer and develop silicon solutions serving the complete end equipment
range from the sensing element, AFE, MCU, communications, signal chain and power management, up to CPUs for the
PLC. TI's real-time Industrial Ethernet technologies are uniquely positioned in wired communications, with
support for all leading industrial standards, enabling manufacturers to tie together different subnets without
the expense of dedicated hardware such as ASICs.
TI has long been an innovator and leader in ultra-low-power technology for wireless communications and
microcontrollers, and is continuing efforts to combine its expertise with energy harvesting to enable advanced
sensors that can operate in places where wiring is impractical. The company is strategically investing and
developing new sensing solutions, including AFEs with the sensing element and analog signal chain integrated.
TI's wide selection of flash- and FRAM-based MSP430™ MCUs brings the flexibility of ultra-low-power
processing to sensors. Since transmission consumes roughly 90 percent of power for a wireless sensor, a sensor
with a processor can save power if it periodically wakes up, samples and measures, transmits, then goes to sleep
again. For a sensor operating on the low power reserve it gains from energy harvesting, such careful power
management is indispensable. Processing also helps sensors that function together determine if one of them has a
malfunction, report the problem, and provide a degree of redundant coverage for the missing sensor.
Data and code protection will be an important issue for networked factories, and individual equipment needs to be
designed with built-in security functions. TI has a history in designing, or helping customers design, secure
embedded systems such as car door locks and wireless encryption schemes. System developers can turn to TI for
enabling expertise in this area as the smart factory continues to develop.
In its different businesses, TI understands and designs to support industrial standards, resulting in products
with voltages, qualifications, temperature ranges, quality levels and packages targeted to industrial
applications. In addition, software and firmware support is available directly or via TI's network of third
parties for issues such as I/O links and Industrial Ethernet protocol stack implementation and qualification.
Applications and system support includes fully documented reference designs with test reports in accordance with
industrial standards.
The company also invests in ongoing research and development and offers dedicated support teams for applications
in industrial systems, factory automation and control, motor drives, smart grid, energy management and building
automation.
A smart future for manufacturing
The same communications advances and embedded intelligence that are bringing networked appliances to consumers
are also having an effect in manufacturing. The main difference, however, is that the systems in factories have
to be more secure, more robust, and operate in real time. In just a few years, intelligent sensors, motors,
robots and other equipments will transform assembly lines and chemical processes, directed by distributed
control that can communicate throughout the factory and, if necessary, around the world. The resulting
revolution in manufacturing will create better products that
are more customized, while keeping costs down, saving energy and reducing waste.
Highly integrated ICs for sensing, control and communications provide the enabling technology behind this
revolution. TI is focused on creating differentiating products, like intelligent hardware and software, as well
as support, that factory equipment manufacturers and manufacturing system integrators will need in the years
ahead. While no one can predict exactly what the smart factory holds for industry, one thing is certain: TI is
playing a leading role and is focused on creating and delivering products that advance the next revolution in
manufacturing.