Mouser Electronics - Electronic Components Distributor
 
Israel - Flag Israel

Please confirm your currency selection:

US Dollars
Incoterms:FCA (Shipping Point)
Duty, customs fees and taxes are collected at time of delivery.
Free shipping on most orders over $100 (USD).
All payment options available

New Israeli Shekel
Incoterms:FCA (Shipping Point)
Duty, customs fees and taxes are collected at time of delivery.
Free shipping on most orders over ₪ 400 (ILS).
Payment accepted in Credit cards only

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


New Tech Tuesdays: Unified Memory Architecture for Mixed Embedded Workloads Mouser Technical Content Staff

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

Embedded systems increasingly rely on non-volatile memory to support a mix of data types, including frequently updated configuration parameters, event logs, and larger firmware images. These varying demands often require multiple memory technologies, including serial electrically erasable programmable read-only memory (EEPROM) for small updates and NOR flash for bulk storage. However, this fragmented approach to memory increases design complexity, raises power consumption, and complicates data management.

Serial peripheral interface (SPI) page EEPROMs offer a unified alternative. By combining EEPROM-like byte-level update flexibility with page- and sector-based erase/program operations and high-speed SPI interfaces, these devices enable a single memory component to handle mixed workloads efficiently. The result is a simpler, more scalable architecture for modern embedded systems.

This week’s New Tech Tuesdays explores how this unified approach replaces the traditional combination of serial EEPROM and flash memory, thereby reducing component count and simplifying both hardware and firmware development.

Unifying Byte-Level Updates and Bulk Memory Operations

A key challenge in embedded design is balancing the need for frequent, fine-grained updates with the efficiency required to store larger data blocks. Traditional EEPROM excels at byte-level updates but is inefficient for bulk operations, while flash memory favors large transfers but complicates small updates.

SPI page EEPROMs bridge this gap. They support byte-level updates and enable page, block, and sector erase/program operations, allowing systems to handle both small and large data updates within a single device.

This capability eliminates the need to split workloads across multiple memory types. Instead, designers can consolidate storage into a unified architecture, simplifying firmware design and reducing the number of external components. For example, a single device can store configuration parameters, log sensor data, and manage firmware updates without requiring separate memory components.

Endurance also improves in mixed-use scenarios. With write endurance typically up to hundreds of thousands of cycles per page, designers can distribute write activity more effectively across memory regions, extending device lifetime while maintaining data integrity.

Optimizing Power and Throughput in a Unified Memory Model

Power efficiency remains a critical constraint for many embedded applications, particularly in battery-powered and always-on systems. SPI page EEPROMs address this with ultra-low-power operating modes, including deep power-down states that significantly reduce standby current while preserving stored data.

At the same time, performance requirements continue to rise. Modern devices in this category are typically organized into 512-byte programmable pages and support high-speed SPI read operations, often reaching tens of megahertz with dual- and quad-output modes. This capability enables fast firmware transfer and data access without changing system interfaces.

Self-timed internal erase and program operations further enhance system responsiveness by allowing the memory device to manage write cycles independently. This reduces processor overhead and improves efficiency during initialization, logging, and firmware updates.

Integrated Reliability and Protection in a Single Device

In addition to consolidation and performance benefits, unified memory architectures deliver dependability through compliance, as they must meet stringent reliability and data integrity requirements. As a result, SPI page EEPROMs integrate several features that enhance robustness in real-world conditions.

Error-correction code (ECC) mechanisms detect and correct memory bit errors, improving long-term data reliability. Additional device-level features, such as Schmitt trigger inputs for noise filtering and high bandwidth memory (HBM)-rated electrostatic discharge (ESD) protection, help improve stable operation in electrically noisy environments.

Data protection features also support system security and traceability. Many devices include dedicated identification pages, unique device identifiers (UIDs), and configurable write-protection regions. Some memory areas can be permanently locked as read-only, safeguarding critical system parameters from unintended modification.

To support safety-oriented designs, these devices may also provide status-monitoring and control features, such as operating status flags and software reset capabilities, helping engineers manage fault conditions and perform system diagnostics more effectively.

The Newest Products for Your Newest Designs®

The M95P family of SPI page EEPROMs from STMicroelectronics provides a practical example of how this unified memory approach is implemented in real-world designs. Available in densities of 8Mb, 16Mb, and 32Mb, these devices combine byte-write flexibility with page-based erase/program operations, enabling both small parameter updates and efficient firmware storage in a single component.

High-speed SPI interfaces with dual- and quad-output modes increase read throughput while maintaining compatibility with existing system architectures. Additionally, ultra-low-power standby and deep power-down modes support energy-constrained applications such as wearable devices and industrial Internet of Things (IIoT) endpoints.

Integrated reliability features, including ECC, protection mechanisms, and secure identification resources, reinforce the value of consolidating multiple memory roles into a single device, thereby reducing the bill of materials and simplifying system integration.

Tuesday’s Takeaway

Modern embedded systems no longer need to rely on multiple memory technologies to meet diverse storage requirements. With SPI page EEPROMs’ ability to update data one byte at a time with fast storage in a single design, these devices simplify embedded systems while improving power efficiency, durability, and reliability.

By consolidating memory functions into a single device, engineers can streamline design decisions and build more scalable, efficient systems. This development is a key advantage as systems continue to scale in complexity and connectivity.



« Back


Mouser Electronics, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.


All Authors

Show More Show More
View Blogs by Date

Archives