New Energy LEDiL Optics Kit (NELOK)

NewEnergy LEDiL Optics Kit (NELOK) is designed to explore LEDiL’s wide range of single-lens solutions that can be used with individual LEDs. This kit comprises a single LED mounted on a Printed Circuit Board (PCB) attached to a heatsink. The PCB is built with a series of precisely placed holes that correspond to the mounting pins of all the members of LEDiL’s single-lens products. With the pins aligned with the holes, this assembly ensures the proper alignment of the lens to the LED for maximal optical efficiency. In addition to the LED/PCB/heatsink, 15 lenses are offered, three each from five lens families. Many secondary optical distributions are also provided for the users through LEDiLs precision molded lens assemblies.

Kit Contents

  • The heatsink/PCB/LED assembly
  • 12” wire harness
  • 15 LEDiL lenses, each packed in a labeled bag
  • A product summary card

The red-black wire harness is stored in a small cavity underneath the heatsink-circuit board assembly. The individual optics are packed in plastic bags. The bottom of the optics typically has an adhesive film designed as an aid for the permanent installation of the optic. In order to experiment with all the lenses in this kit, affix the lenses with the lightest possible pressure.

Using the Kit

Connect the wire harness to the PCB, pushing one of the tinned ends of the harness into each of the poke-in wire connectors. The LED requires a 3VDC power supply. The LED will light up with the delivery of 15mA of current. The max current rating for the XP-G3 S-Line is 1500mA. The PCB has pin holes to support the placement of every lens family in the LEDiL product line, which might be confusing. The pin holes for all the LEDiL optics in this kit are 2mm holes at 8.6mm center-to-center.

Mechanical Dimensions

Mechanical Drawing - New Energy LEDiL Optics Kit (NELOK)
Chart - New Energy LEDiL Optics Kit (NELOK)
Published: 2023-08-11 | Updated: 2026-02-10