Mouser Electronics Inks Global Distribution Agreement with Morse Micro for Long-Range Wi-Fi HaLow Solutions

For Immediate Release

Connect With Us


March 18, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announced a global distribution agreement with Morse Micro, the leading Wi-Fi HaLow® silicon vendor. Through this agreement, Mouser is now stocking Morse Micro's long-range, ultra-low-power Wi-Fi HaLow modules and development platforms.

Morse Micro's comprehensive portfolio includes the industry's smallest, fastest and lowest power Wi-Fi HaLow SoCs and modules, providing 10x the range, 100x the coverage area and 1000x the volume of traditional Wi-Fi solutions. Designed specifically for the Internet of Things (IoT), Wi-Fi HaLow operates in the sub-GHz frequency band, offering an optimal combination of extended range, power efficiency, long battery life, superior penetration of barriers, large network capacity, and advanced security. Targeting commercial, residential, and industrial IoT markets, Morse Micro's Wi-Fi HaLow solutions are ideal for access control, security cameras, industrial automation, and retail and mobile device applications.

Morse Micro products now available through Mouser include the MM6108-MF08651-US Wi-Fi HaLow module. This fully integrated Wi-fi HaLow module offers long-range, low-power consumption and superior RF performance and features Morse Micro's MM6108 Wi-Fi HaLow SoC. The MM6108-MF08651-US module simplifies Wi-Fi HaLow implementations by using an integrated Power Amplifier (PA), low-noise amplifier (LNA) and a transmit-receive switch (T/R).  The module is FCC certified for operating on frequencies between 902 MHz and 928 MHz, achieving a maximum data rate of 32.5Mbps. The MM6108-MF08651-US module is ideal for transitioning from previous RF technologies and supports the latest WPA3 security protocols for secure, long-range applications.

Morse Micro's MM6108-EKH03 Wi-Fi HaLow development platform, also available from Mouser, supports a Linux SDK based on OpenWrt to provide seamless connectivity through a range of applications and software for secure and efficient development. Equipped with a Wi-Fi HaLow to Ethernet/USB adapter, a 100Mbps Ethernet port and a USB port, MM6108-EKH03 can be configured directly via the host AP web interface, providing an integrated and simplified configuration experience. The built-in web-based configuration wizard makes configuration and operation truly frictionless.

The Linux-based MM6108-EKH01 Wi-Fi HaLow development platform simplifies evaluation with a versatile set of interfaces, including USB-A for console access, Ethernet ports, and a Micro-HDMI port for display. It further offers expansion capabilities, allowing the addition of a camera module, which enhances its functionality.

To learn more about all the Morse Micro solutions available from Mouser, visit https://www.mouser.com/manufacturer/morse-micro/.

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Morse Micro

2026 - Morse Micro builds a new generation of wireless chips that reach farther, are lower power, and are genuinely secure. The company is a dedicated contributor to the Wi-Fi Alliance's efforts to bring interoperability certifications for Wi-Fi HaLow technology to the market. Morse Micro serves commercial, residential, and industrial IoT markets, with applications including access control, security cameras, industrial automation, and retail and mobile devices. The company's turn-key solution enables a whole new range of smart devices to connect wirelessly.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764