Mouser Electronics Expands Antenna Range with New Embedded, Flexible and External Wi-Fi 6E Solutions

New Product Announcement

Connect With Us


Spotlight: Wi-Fi 6E Antenna Solutions

January 9, 2024Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, broadens its range of antennas designed for high-speed Wi-Fi 6E communication.

The introduction of IEEE's 802.11ax wireless standard brought forth several technical initiatives aimed at advancing connectivity for the next generation of devices. One key addition was the inclusion of Wi-Fi 6E, enabling Wi-Fi communication on the 6GHz spectrum for the first time. By operating at frequencies above the existing 2.4 and 5 GHz networks, Wi-Fi 6E enables better optimization, less interference, and lower latency. Security is also enhanced, as Wi-Fi Protected Access 3 (WPA3) certification is mandatory for all Wi-Fi 6E devices. Since its introduction in 2020, the deployment of Wi-Fi 6E has expanded to a diverse range of industrial and consumer locations, including offices, manufacturing facilities, clinical environments, and residential areas. Consequently, supporting Wi-Fi 6E has become essential for the latest high-performance wireless devices.

Mouser stocks a wide range of antenna designs needed to fulfill the diverse technical requirements of Wi-Fi 6E devices. Some of the newly added solutions include:

  • The UAM Wi-Fi® 6E/Wi-Fi 7 Embedded Antennas from Linx Technologies / TE Connectivity are an innovative range of omnidirectional tri-band antennas designed for the latest Wi-Fi 6E devices. As an externally mounted solution, they can be easily attached to a metal chassis using the unique snap-in feature, removing the need for fixings, allowing for unambiguous mounting direction, and increasing assembly speed. Alongside Wi-Fi 6E functionality, they allow for wireless Bluetooth® and ZigBee communication, as well as supporting future Wi-Fi 7 networks. The RoHS-compliant range includes multiple cable lengths, with MHF4l and MHF termination available, and is suitable for a wide range of indoor applications.
  • The Tri-band Wi-Fi 6E Flexible Printed Antenna from Abracon provides high-performance communications in low-profile and easy-to-integrate packaging. The omnidirectional tri-band operation provides high performance across 2400MHz to 7125MHz frequencies, covering vital 2.4 GHz, 5 GHz, and 6 GHz bands. The antenna helps to enhance the range of Wi-Fi signals, providing dependable and high-speed connectivity in congested public spaces and complex industrial settings. In conjunction with Wi-Fi 4/5,6/6E and 7 connectivity, it is also ideal for devices using Bluetooth, ZigBee, Thread, and Matter protocols. System assembly is straightforward, with the flexible design allowing for quick adhesive mounting even along contours. The antenna is suitable for a variety of routers and network devices, as well as home automation and IoT sensors.
  • Kyocera AVX's range of antennas includes solutions designed to suit a variety of Wi-Fi-connected applications. The FR4-based WXP3015W08 antenna features an embedded Wi-Fi dipole design and delivers high-performance connectivity and signal sensitivity in miniaturized packaging. It consumes minimal space and can easily be mounted through simple adhesion. For Wi-Fi 6E connections, it features a peak gain of 5.90dBi and an average efficiency of 60%, ensuring a strong connection. It is also suitable for previous iterations of Wi-Fi, as well as Bluetooth, BLE, and ZIGBEE protocols. Kyocera's RoHS-compliant AVX range also includes stamped metal and flexible printed circuit Wi-Fi 6E antennas, which use its patented isolated magnetic dipole (IMD) technology, as well as several cable lengths and termination options.

In 2023, Mouser launched more than 66,000 part numbers ready for shipment, including over 8,000 in the fourth quarter. To see more new innovative products, visit https://info.mouser.com/new_products/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764