Samtec APF6 & APM6 AcceleRate High-Performance Terminals Now at Mouser

New Product Press Brief

Connect With Us


August 4, 2022 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking APF6 and APM6 AcceleRate® high-performance terminals from Samtec.

Samtec APF6 and APM6 AcceleRate® terminals are 0.635 mm pitch interconnects featuring 112 Gbps PAM4 extreme performance and a flexible open-pin-field design. The APF6 and APM6 AcceleRate terminals have a high-density, four-row design, with 10 to 100 positions in each row. These devices are ideal for space-constrained applications, with slim, low-profile dimensions of 5 mm × 5 mm.  

The Samtec APF6 and APM6 AcceleRate terminals support 56 Gbps PAM4 (28Gbps NRZ) applications and are PCIe® Gen 5 compatible.

For more information, visit https://www.mouser.com/new/samtec/samtec-apf6-apm6-accelerate-terminals/

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764