Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

WiFi and Bluetooth Coexist with the Atmel WINC1500 Low Power WiFi Module Now at Mouser

March 12, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now shipping the new WINC1500 Wi-Fi Module from Atmel Corporation. The WINC1500 is a low-power consumption 802.11 b/g/n WiFi module specifically optimized for low power Internet of Things (IoT) applications. The WINC1500 WiFi module supports WEP, WPA, and WPA2 WiFi security encryption as well as China WAPI security while drawing as little as 4µA. This module includes features that allow both WiFi and Bluetooth signals to coexist locally without any signal interference.

The Atmel WINC1500 Wi-Fi Module, available from Mouser Electronics, is a highly integrated device featuring a small form factor at only 21.5mm x 14.5mm x3.4mm. This module includes an integrated power amplifier, low noise amplifier (LNA), all necessary power management functions, and an integrated antenna. This module targets low power WiFi wireless applications and draws only 4µA in Deep Power Down mode. When in beacon monitoring mode the module draws only 850µA in Doze Mode. This module provides SPI, UART, and I2C host interfaces for communicating with a host microcontroller. It also supports 2-wire and 3-wire Wi-Fi/Bluetooth coexistence signaling interface. The interface allows this module to coordinate transmission and reception with a compatible Bluetooth module to insure that both radios do not interfere with each other.

The Atmel WINC1500 is based on a powerful Cortus-APS3 32-bit processor. This processor performs hardware accelerated MAC functions including association, authentication, power management, security key management, and MSDU aggregation/de-aggregation. In addition, the processor provides flexibility for various modes of operation, such as STA and AP modes. An on-chip IP stack minimizes the host microcontroller requirements and supports TCP, UDP, DHCP, ARP, HTTP, SSL, and DNS.

To learn more, visit: http://www.mouser.com/new/atmel/atmel-winc1500/ .

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser Electronics
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

About Atmel
Atmel Corporation is a global leader in designing, manufacturing and marketing advanced semiconductors including microcontroller (MCU), programmable logic, and nonvolatile memory. By combining these core technologies, Atmel meets the evolving and growing needs of today's electronic system design engineer through the production of general purpose and application specific system level integrated chips. Atmel's world class expertise and wealth of experience in system-level integration enable all of Atmel's products to be developed from their constituent blocks with minimum delay and risk. 

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Corporate Communications Manager
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room