Build Long-Range IoT Networks with Microchip's RN2903 LoRa Transceiver Module, Now at Mouser
June 22, 2016 - Mouser Electronics, Inc. is now stocking the RN2903 LoRa® transceiver module from Microchip Technology. The RN2903 is a LoRa-integrated modem with a range of more than 10 miles (15 km), low power consumption that enables a battery life greater than 10 years, and the ability to connect millions of wireless sensor nodes to LoRa gateways and Internet of Things (IoT)-connected cloud servers. LoRa technology's unique spread-spectrum-based modulation is capable of demodulation 20 dB below noise level, which enables high sensitivity for ultra-long range, improved network efficiency and eliminates interference.
The Microchip RN2903 LoRa transceiver module, available from Mouser Electronics, operates over the 915 MHz license-free Industry Scientific and Medical (ISM) frequency bands and serves as the end-device in the LoRa network infrastructure. The RN2903 has the complete LoRaWAN™ protocol stack on the modem and is easy to configure via simple ASCII commands through the UART, greatly reducing development time. The RN2903 is FCC-certified, saving significant certification costs. Additionally, it combines a small form factor 17.8 × 26.7 × 3 mm with 14 general-purpose inputs and outputs (GPIOs), providing the flexibility to connect and control a large number of sensors and actuators while taking up very little space.
With the RN2903 modem, wireless developers can maximize both longer range and lower power, while eliminating the cost of additional repeaters and increasing battery life. The module integrates radio frequency (RF) communication, a baseband controller, and a command application programming interface (API) processor, making it a complete long-range solution with an external host microcontroller. With its scalability, robust communication, mobility, and the ability to operate in harsh outdoor environments, the RN2903 is well suited for a broad range of low-data-rate wireless monitoring and control designs, such as energy metering, location tracking, utility infrastructure monitoring and control, and agriculture.
To learn more, visit http://www.mouser.com/new/microchip/microchip-rn2903-module/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 22 global support locations and stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 600 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Microchip Technology
Microchip Technology Inc. is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com