Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

TI's LMZM2360x Step-Down Power Modules, Now at Mouser, Offer High Efficiency and Industry-Leading Space Savings

July 19, 2018 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader empowering innovation, is now stocking LMZM23600 and LMZM23601 step-down DC-DC power modules from Texas Instruments (TI). Housed in a compact, 3.8 mm × 3 mm × 1.6 mm MicroSiP™ package, the modules can reduce board space by up to 58 percent, making the LMZM23601 the smallest 1 A DC/DC power module on the market for industrial applications.

TI's 0.5 A LMZM23600 and 1 A LMZM23601 power modules are available from Mouser Electronics in a fixed-output voltage of either 3.3 V and 5 V or with an adjustable output voltage of 2.5 V to 15 V. The modules feature an integrated inductor and an input voltage range of 4 V to 36 V with up to 92 percent efficiency to minimize energy loss. The modules' 30 µA quiescent current increases light-load efficiency and extends battery life in battery-powered applications.

The LMZM2360x power modules require only two external components for fixed-output voltage performance, offering an easy-to-use solution for designers, as well as plug-and-play capability. The power modules support a seamless transition between forced PWM mode and auto PFM mode, enabling both constant-frequency operations and high-efficiency operations with light loads. The modules are optimized for low-EMI, performance-driven industrial applications and include built-in control loop compensation, soft start, current limit protection, and undervoltage lockout.

The LMZM2360x modules are supported by the LMZM23600 and LMZM23601 evaluation modules, fully assembled and tested modules that allow developers to evaluate the features and performance of the power modules. The LMZM236000 evaluation module is available in all three output voltage options, while the LMZM23601 evaluation module is available in an adjustable 2.5 V to 15 V version.

The LMZM2360x power modules are ideal for space-constrained designs such as sensor transmitters, grid infrastructure, field transmitters, ultrasound scanners, and network security cameras. To learn more about the LMZM236000 power module, visit www.mouser.com/ti-lmzm23600-power-modules. For more information on the LMZM236001 power module, go to www.mouser.com/ti-lmzm23601-power-modules.


With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room